Modern construction faces a challenge. The average risk of musculoskeletal disorders (MSDs) is continually higher for people in this line of business than for people in all other industries combined. However, improving ergonomics can help overcome this challenge. For this purpose, LINAK actuators ensure a smooth cab ingress and egress when installed in powered retractable access systems.
Even though about 90 per cent of small US construction companies have a safety programme, only a third of them have an ergonomics programme. This, combined with an estimated annual wage and salary loss of $46 million in the private US construction sector, creates an incentive to invest in ergonomic solutions.
Safe and ergonomic cab entry/exit with adjustable ladders
 Adjustable ladders – or other powered retractable access systems – ensure a safe extension/retraction, bringing the ladder closer to the ground. For the machine operator, this provides a safer and more ergonomic way in and out of the cab with visible and angled steps. It will also spare the driver’s knees from strain as the first step is closer to the ground.

By improving ergonomics, you are likely to reduce the amount of working days lost due to MSDs. In the UK alone, this represents 6.6 million working days a year and a total of 469,000 workers, all suffering from MSDs (new or long-standing).
The system offers several benefits
 For the entrepreneur, there are also other benefits of a powered retractable access system. Adjusting the ladder with actuators powered by battery means that the dependence on the hydraulic system is gone, and the ladder system is operable when the main engine is not running. All you need is power from the battery and a remote control. 
Furthermore, the system can be used as an additional theft/vandalism precaution – as accessing higher cabs will be complicated without an extended ladder. According to ISO 2867:2011, the ladder must be activated and fully extended to allow access to the cab.
Ergonomics matters – also in construction!
If you want to know more about what LINAK can do for construction vehicles, visit the construction business area site. You are also welcome to contact your local LINAK office for more information.