These electric dual actuators, embodied by the TWINDRIVE® concept at LINAK®, empower furniture designers with unparalleled design freedom and performance capabilities in crafting comfort furniture solutions. This multi-actuator technology provides performance benefits such as leg adjustment and bed control.
LINAK TWINDRIVE systems for adjustable beds
Our dual actuators are called LINAK TWINDRIVE systems, and they provide a comprehensive solution for adjustable beds. You will enjoy maximum free space beneath your electric bed, as well as a range of integrated features. Just connect the dual actuator system to power and pair it with your preferred control - whether it's a wireless hand control or an app. Operate your bed however you see fit!
The beauty of the LINAK dual actuators lies in their all-in-one design. Everything is integrated within the dual actuator, eliminating the need for many components in a system. Even better, advanced versions of the dual actuators offer additional features, such as memory function and the ability to add accessories. You can even opt for the parallel drive of two beds, making these systems the ultimate solution for comfortable and convenient adjustable bed setup.
One dual actuator – two adjustments
TWINDRIVE electric dual actuators, also known as double motors, are most used in adjustable comfort beds for residential use. These provide the option of two distinct adjustments for the bed, while only requiring the installation of one actuator onto the bed frame.
Dual actuator systems for adjustable beds
The LINAK dual actuators, or TWINDRIVE, are the all-in-one solution for incorporating movement into an adjustable bed. We have optimised our dual actuators to ensure compatibility with most dual actuator bed frames, using standardised spacing between crossbars and universal twist bracket dimensions/designs found in the market.
To mount a TWINDRIVE dual actuator, it needs to be installed on crossbars located on the bed frame. To ensure that the rotational movement produced by the dual actuator creates the appropriate movement of the bed, twist brackets are attached to these crossbars. The actuator then pushes the twist bracket to rotate the crossbar, thereby moving some part of the adjustable bed.

Accessories and advanced technology for dual actuators
At LINAK, modern adjustable comfort beds come with Bluetooth® technology – enabling wireless control of the movements. Hand controls or an app will pair to the product via Bluetooth and provide wireless control. Consumers can download the LINAK Bed Control App or one of our customers’ customised apps to control their furniture using a mobile device as a hand control.
The advanced versions of TWINDRIVE dual actuator also allow for the connection of an accessory to the system. This can either be a massage motor or the LED light rail for even more under-bed light.
The Bluetooth® word mark and logos are registered trademarks owned by Bluetooth SIG Inc. and any use of such marks and logos by LINAK® is under license.
Frequently asked questions
How to set up a double bed for simultaneous drive with the TD4 Standard or TD5 Standard.
The system consists of:
2 x TD4 Standard (Can also be two TD5 Standard)
2 x mains cables
1 x Bluetooth® hand control
- Connect the two dual actuators TD4/TD5 to the mains
- The Under Bed Light on both TD4/TD5 dual actuators starts to flash to indicate pairing mode
- Pair the hand control (press the two top buttons simultaneously)
- A long flash indicates successful pairing
- Now both dual actuators TD4/TD5 Standard are paired to one hand control
The question about which dual actuator is best depends entirely on the bed you want to integrate movement into. Therefore, it is not possible to say which LINAK dual actuator is best for your bed design.
First, you will need to know how much force your bed design requires. For heavy constructions and mattresses, we recommend TD5, whereas for slatted beds with lighter mattresses, we recommend TD4.
Secondly, you will need to know which features you want your bed to have. For all the standard features the standard version of the dual actuator is fine. However, should you require an extra actuator, parallel drive of two beds, and also want to offer the possibility of saving favorite positions, you will need an advanced dual actuator.
To find out exactly which system fits your requirements, our sales people are always ready to help you find the right solution.
Beds can be designed in many ways, but for adjustable beds the choice is typically between single actuator systems, dual actuator systems or a combination of both. However, the bed frames for each of these systems are very different.
For electric dual actuator systems the bed frame simply needs to have the standard spacing between the crossbars responsible for adjusting the back or leg part of a bed. This crossbar must also have twist brackets mounted so the dual actuators have something to push to make movement.
In this video you can see how mounting happens.
Dual actuators from LINAK only use wireless control options. The integrated Bluetooth® communication allows you to pair the electric actuator system with either one of our wireless hand controls, the LINAK Bed Control App or your own customised app.
Watch the TWINDRIVE TD4 instructional video to learn more about the innovative mechanical emergency lowering feature. This procedure also apply to our TD5 dual actuators.
At LINAK we work with two types of dual actuators: Standard and Advanced.
The Standard versions offer back and leg adjustment with only one unit as well as the following integrated features: mechanical emergency lowering, low stand by power consumption and integrated under bed light.
The Advanced versions of the LINAK dual actuator offer the same features as the Standard version – and then something extra. In addition, they offer the option of parallel drive of two beds, the possibility of saving favourite positions and adding extra accessories such as massage motors or extra under bed light.
You can tell the Standard and Advanced versions apart by looking at the plugs. If there is an available plug after having connected the power cord – you have an advanced version.
The LINAK® dual actuators, or TWINDRIVE®, is an all-in-one solution where one unit offer two separate adjustments of a bed. The dual actuators are used to incorporate movement into an adjustable bed. We have optimised our dual actuators to ensure compatibility with most dual actuator bed frames, using standardised spacing between crossbars and universal twist bracket dimensions/designs found in the market.
A dual linear actuator is mounted on crossbars with twist brackets on. This means that the rotational movement created by a dual actuator pushes the twist bracket in a way that rotates the cross bar which then in turn moves some part of an adjustable bed.