Electric linear actuators can be used in more types of residential furniture than most people realise. Best known as an actuator for residential seating such as recliners, armchairs, or sofa recliners, the LA10 is a good example of this.
The same benefits that apply to seating also apply to adjustable beds and other furniture. The LA10 actuator was developed to fit into small spaces and minimise the number of components required during assembly. Only a few cables are required, and they are easy to manage.
These points have been raised by various seating brands and manufacturers, and they are challenges that any furniture designer will recognise.
Advantages of the LA10 electric linear actuator
Design freedom with a small actuator
Designers can envision slim and sleek adjustable bed designs without having to make room for bulky actuators. The LA10 is relatively compact and can be discreetly integrated into most designs without compromising strength or reliability – enabling new design opportunities and helping optimise production.
Fewer parts, fewer cables, fewer issues
There is no need for a separate control box or multiple types of actuators to complete the system. The control box is integrated into the actuators, and all LA10 actuators are designed to connect in a series. Power line communication reduces the number of cables. Only one cable is needed per actuator, along with a power cord. This makes installation faster and reduces the risk of cable clutter.
Storage that makes sense
Storage is easy to manage with this actuator, as the system consists of only a few components. This means fewer components to store and an actuator that can be easily connected with a single cable and used across various types of furniture.
Simplify assembly in production
As a plug and play system with few components, the LA10 system is easy to assemble and ready for installation. This saves time in production, where assembly and mounting can often be time-consuming.
In summary, the LA10 electric linear actuator system is a compact solution for movement in recliners, chairs, sofas, accessibility furniture, cinema seating, and similar applications.