Skip to main content
Why ergonomics matters in construction machinery

In the UK alone around 80,000 construction workers suffer from illnesses they believe were caused or aggravated by their daily job. According to the British Health and Safety Executive (HSE), 65 % of these ailments are cases of so-called Musculoskeletal Disorders – or MSDs.

A total of 6.6 million workdays are lost due to MSDs in the UK each year, and more than a third of these are back disorders (40 %). Naturally, this is costly. An estimate from the British Institution of Civil Engineers states that MSDs in British Construction costs employers £646 million annually. However, improving ergonomics can help bring that number down.

Improve working postures to minimise MSDs
Poor working postures are one of the culprits when it comes to MSDs – also within construction. For example, hours of sedentary work inside the driver’s cab of a construction vehicle is a recipe for MSDs. However, several easily implemented initiatives can help lighten the burden on the drivers and increase their comfort. Just allowing the construction worker to adjust the control panel, in order to vary their working positions between sitting and standing, improves the situation significantly. 

Why ergonomics matters in construction machinery
Adjustable cabine pult

This has, for example, been the case for the Swedish-based mining-tech expert, Sandvik, who have implemented several adjustment options to some of their large construction machinery.

“Improved ergonomics is a clear indicator of the fact that Sandvik wants to develop and offer the best quality operator environment in the world,” says Mika Väisänen, Project Engineer from the Product Development Department at Sandvik Mining and Rock Technology. 

Read the full story with Sandvik.

Several adjustable solutions to improve ergonomics
It is all about fitting the job to the employee. Construction workers and drivers of construction vehicles are as different in size and shape as the rest of us, and the workstation needs to be flexible to fit the person operating it.

LINAK already offers electric actuator solutions to adjust control panels, accelerator, brake and clutch pedals, as well as seats – all to enable personalised settings for the driver to avoid painful MSDs, and to help entrepreneurs minimise loss of workdays. All our actuator solutions are characterised by easy installation – even when space is limited. Compact products and only a few cables make integration painless too.

Ergonomics matters – also within construction! 

If you want to know more about what LINAK can do for construction vehicles, visit the Construction solutions site. You are also welcome to contact your local LINAK office for more information. 

Related products

Related applications