A custom-built solution
Initially, the team explored the Danish market for a complete plug‑and‑play solution. As Supply Chain Manager, Berit Timm Sørensen, explains: “We were not able to find a supplier offering exactly the solution we were looking for. So, we decided to do it ourselves – after all, we have the right competencies in-house for a task like this.”
Warehouse assistant Carsten Skovhus led the project. With 20 years of warehouse experience, optimisation is a natural part of his work. Carsten produced the first sketches for the new setup and gathered input from colleagues along the way. The drawings were then handed over to the in-house carpenter, who built the setup – reusing lifting columns and other materials already available in the warehouse.

Ergonomics in every detail
The team soon had two new packing workstations ready, each carefully designed with ergonomics in mind. As Carsten explains: “The workstations are height‑adjustable, which is essential as my colleagues range from 160 to 198 cm in height. We also focused on keeping frequently used items close at hand, helping reduce unnecessary bending, twisting or stretching.”
Carsten highlights the computer module: “We placed the computer and label printer on a separate module. This module is height adjustable as well and operated using a foot switch, so there is less need to bend. The module also has an additional lifting column that raises the keyboard section when there is a need to change label rolls. It is a practical and functional solution.”

A result that makes a difference
Shortly after the new workstations were put into use, warehouse assistant Pia Wils Nielsen shared her experience: “This is one of the best improvements in my 12 years at LINAK.”
Pia already notices the benefits: “I no longer feel discomfort in my body, and everything I need is within easy reach.”
Carsten agrees: “I am pleased with the result. The setup is straightforward to work at, and we reduce time spent walking back and forth to fetch items.”
Berit sees clear value in the new solution as well: “It has been a really good process. These packing workstations are built on the employees’ experience, and the result is a setup with smart solutions. I believe it can support wellbeing and long-term job satisfaction.”

Continuous improvement
At LINAK Denmark, ergonomic optimisation is an ongoing process. The next step in the warehouse is to make the computer module mobile, enabling it to be moved easily when packing large shipments away from the main workstations.
Are you also considering improving ergonomics at your workstations? Explore our range of lifting column kits for height‑adjustable industrial workstations – including plug‑and‑play lifting column kits, or contact us for guidance on which columns best suit your needs.