Skip to main content

The basic components of an electric actuator are a motor, a gearing, and a spindle. However, sometimes a clutch mechanism is added to the actuator design. In this video, our expert Hunter Stephenson explains the purpose of a clutch in an industrial linear actuator, and how the clutch works in the LINAK® actuator LA36.

Did you know?

The clutch serves two purposes in an actuator. One is to protect the industrial machinery and the actuator. The other is to ensure that the actuator can be used without control electronics.

A linear actuator with a clutch mechanism offers great versatility, making it easier to implement the actuator in different machinery.

The clutch protects the actuator and the application in case of overload by disengaging the rotational movement from the motor to the gear and spindle when the torque exceeds a pre-set limit. This safety feature is related to the rotational movement of the motor and therefore it only works when the actuator is running. If you would like to know more about the function of the clutch, check out the video above.

Got a question?
If you have questions about our actuator components, feel free to contact your local LINAK office.

Related topics