select
Desk Control Basic SW

Desk Control Basic SW

Desk Control Basic is a DESKLINE® software desk panel for use in all types of office desks. The Desk Control Basic software is to be installed in your computer (PC or MAC) making the use/adjustment of your desk very intuitive in your daily work. The software program contains the typical desk panel features like up, down adjustment, up to 3 memory positions and height read-out. Additionally, the program reminds you to adjust your desk, counting the time standing as well as the calories burned. –The intervals are self-elected making Desk Control Basic a very personal tool.

Desk Control Basic works with all LINAK DESKLINE systems. Simply connect the USB2LIN06 cable between your control box and your computer and download the Desk Control Basic software. If you prefer a wireless connection, plug the Bluetooth® Adapter in your control box and download the Desk Control Basic software. Optional it is possible to connect a standard desk panel to the system to ensure adjustment of the desk while the computer is turned off.

This software is for users using the USB2LIN cable, Windows 7 or computers without Bluetooth®. If you have Windows 8.1 or newer and Bluetooth® communication, we recommend downloading the Desk Control™ App instead. 

Download the Desk Control Basic software here.
Desk Control Basic SW

Desk Control Basic SW

View the data sheet as an online magazine or download the PDF.

Online Magazine | PDF

No 2D drawings available. 

No 3D models available.
Desk Control Basic is software that controls the desk movements, but at the same time encourages users to increase active movements while working.

Select any of the applications below to download free Desk Control Basic software.

Requirements

  • Communication between PC/Mac and the CBD control box requires a USB2LIN cable from LINAK.

Supported Operating Systems

  • Windows 7 (with .NET version 4.5)
  • Windows 8 or higher Operating System
  • Mac OS (OS 10.7 or higher Operating System)
Download:

 

Desk Control Basic SW User Manual

Desk Control Basic SW User Manual

This User Manual will tell you how to install, use and maintain your LINAK DESKLINE® products.

Online Magazine | PDF

Trouble Shooting


  1. The desk does not drive at all
  2. The desk can only drive downwards
  3. How to store a memory position
  4. The height in the display is not correct
  5. The desk will not drive the full stroke upwards. Always stops in the same position
  6. The display shows E01 error code instead of the height
 

The desk does not drive at all


Check: Is the mains connected to the control box?
Try/Solution: Try to connect a lamp or similar to the mains supply to check that the supply voltage is OK.

Check: Are all plugs mounted correctly in the control box and to the leg?
Try/Solution: Check all connections.

Check: Are there any visible damages on cables, controls, the control box or legs?
Try/Solution: Damaged parts must be exchanged – contact the company where you bought your desk.

Back to top.


The desk can only drive downwards



Back to top.


How to store a memory position


  • Favourite positions e.g. for sitting and/or standing can be stored. Follow the procedure shown in the video or in the text below.


How to store a position

How to store:
1. Drive to the height you wish to store
2. Press ‘S’ and then the memory button
Your position has now been stored

To recall your memory position, press the memory button until you reach the stored position.

- Download above video: How to store a position (21Mb .wmv-file)

Back to top.


The height in the display is not correct


  • Correct the height in the display to the actual height of the desk by following the procedure shown in the video or in the text below.


How to set the height of your desk (DPF1C)
Set the height:
Measure the actual height of your desk – from floor to the upper edge of the tabletop

Set the height:
1. Press the up and down keys at the same time
2. A figure appears in the display
3. Use the up or down key to change the figure to the actual height

- Download above video: How to set the height of your desk - with DPF1C (16Mb .wmv-file)

Back to top.


The desk will not drive the full stroke upwards. Always stops in the same position

 
  • The system has set a new end-stop outwards. To erase this position, the desk must be initialised again. Follow the procedure shown in the video: How to initialise your desk.

Back to top.


The display shows E01 error code instead of the height


  • There is a malfunction in the desk. Error code E01 means that the desk must be initialised. Follow the procedure shown in the video: How to initialise your desk.

Back to top.


YouTube video - "How to initialise your desk":


How to initialise your desk
The desk cannot drive up if it has not been initialised
If display: error code E01

How to initialise:
1. Press down key and drive to the lowest position.
Hold the key until the desk stops completely

2. Reactivate the down key and hold the key until the desk stops completely.
Now the desk can drive up.

- Download above video: How to initialise your desk (16Mb .wmv-file)

Back to top.
For further information please see the DESKLINE User Manuals.
What is a Control
The control is a unit used to control the movements of a LINAK actuator system…
DESKLINE Applications
See examples of DESKLINE applications.
Subscribe to News
Stay up to date with News from LINAK.
Move to Improve
Moving is a part of life. And, it should not stop at the door of the office.
Contact LINAK
Need assistance finding the product that fits your specific requirements?