select
 

What you need to know about the battery BA001

LINAK Sales Engineer Stefan answers frequently asked questions about the LINAK battery BA001. The battery supplies power to an electric actuator solution. In short, it replaces the need for a power cord connected to the mains when you make adjustable mobile furniture.

Corporate News:  08 May 2017

Stefan Lorenzen is a Sales Engineer from LINAK A/S in Denmark. Along with all his colleagues, he knows everything there is to know about the battery BA001 from LINAK. Every day, he answers questions about LINAK products. He now shares the answers to the most frequently asked questions about using the BA001 in furniture design.

Why should I use a battery instead of a mains cable?  
Easy ergonomic electric adjustment as well as increased mobility becomes possible by including a battery in a piece of furniture with electric adjustment. 

How many times can a battery run furniture up and down?
 
This depends on the actuator solution and the kind of furniture with which you equip the BA001

If we look at, for instance, an ergonomic library cart it will run around 160 full cycles up and down on one charge* - In other words, it will easily last through several workdays for a librarian. On a regular height adjustable office desk with two legs and an average load the battery will run around 40-50 full cycles on one charge*. 

How do I see the battery power level? 
The battery has an intuitive status indicator where LED bars indicate the capacity level. An audio alarm also beeps when it hits 25 percent capacity to alert you that it is time to recharge soon. 

What do I do if it runs out of power?
 
Charge the battery or replace it with a charged battery. With flexible charging, you just plug a mains cable into the control box on the furniture and leave it to charge overnight. It will be ready in the morning. 

You can also click off the battery BA001 and recharge it via an external power source. 
  Stefan Lorenzen, LINAK Sales Engineer at LINAK A/S in Guderup, Denmark.
How do I replace the battery?
This is easy. A practical bracket makes it simple to click the battery on and off when you want to replace it. The bracket is always included. 

Does it use power when it is not in use?
The BA001 has ZERO™ technology, which ensures that it has a standby power consumption lower than 0.1W when not in use.

Where do I mount the battery?
Mount the battery next to the control box in a solution. The BA001 also has integrated wire management where practical grooves on the back of the battery can manage and fixate wires when mounted.

* Depends on the load. Small adjustments during the day count as partial cycles - not as a full cycle.


Be Mobile   Be Mobile with the BA001
The mobility, which a battery offers to a solution, broadens the number of places where we can think mobility and ergonomics. 

For additional inspiration, see our BeMobile inspiration folder.  

 

For further information, please contact your local LINAK subsidiary or distributor.


We provide innovative actuation solutions that improve people’s quality of life and working environment.

We will be the global leader in innovative electric actuator systems within our core segments.

Updated: 08 May 2017 06:56