Contact us here
News 14 July 2017

New design increases LINAK Bed Control App usability

LINAK improved the user-friendliness of the Bed Control App while giving it a contemporary look, a new app icon, and making the user interface as intuitive and simple as possible.

New design increases LINAK Bed Control App usability

User-friendliness was a top priority when the Bed Control App had an upgrade – both in terms of design and functionalities. The new design is user-friendly, light, and simplified so that the functionalities are highlighted. Not only does the app automatically recognise the product it is connected to, it is also easier to store and locate memorised positions in the app. As if that was not enough, the app initiates by presenting an easy guide of how to pair the product with your phone. 

Intelligent app – you only need one
The Bed Control App is now intelligent. This means that the app automatically recognises the features of the product it is connected to. What is more, the graphics in the app will align with the relevant product. Take for instance memory positions: If you connect to a TD4 Standard, the app will show the standard back and leg adjustment, whereas it will also display four memory positions if you connect it to a TD4 Advanced.

New design increases LINAK Bed Control App usability
 

This is also why we only need one app now. Previously, your customer had to locate the right app, choosing between an app with memory and an app without, but now one app is all they need. 

Onboarding flow
As a new feature the app will initiate by showing the user an onboarding flow of how to initiate pairing mode in the product so you can pair it with a phone. By following a few steps on the screen, the user is able to easily pair the phone and product and then adjust the bed to the degree that the product allows. 

What do I have to do? 
Do not worry. The next time your customers update their Bed Control Memory App they will automatically get the updated version of the app. Other than updating the app, your customers do not have to do anything actively. 

Bed Control App functionalities

  • Adjustment of back and leg
  • Simultaneous drive
  • four memory positions - if supported by the product
  • Turn Under Bed Light on/off
  • seven languages (English, Danish, Korean, French, German, Spanish, Italian)
  • Compatible with the Bluetooth® Adapter and the TWINDRIVE® TD4

Do you want to try the Bed Control App? Download it for both iOS and Android. 

New design increases LINAK Bed Control App usability Apple Store Google Play


Got a question?

Our team is ready to assist you with technical information, starting a project and more.