select
HC20 Wireless

HC20 Wireless

The wireless hand control HC20 is designed for use with LINAK TWINDRIVE® or CBH Advanced systems for leisure beds.

The hand control is based on RF (Radio Frequency technology) or Bluetooth® connection. It has a contemporary design that matches the trend within interior design.

The HC20 combines ergonomic design and functionality into a user-friendly hand control without any annoying cable. As standard the HC20 offers memory, backlight in the buttons for extra user-friendliness and torch function. 

Hand Control HC20 Wireless Data Sheet

Hand Control HC20 Wireless

View the data sheet as an online magazine or download the PDF.

Online Magazine | PDF

TWINDRIVE® TD4 – Wireless is the new standard

Explore the TD4, specially developed for comfort beds with a moderate need for power.

Online Magazine | PDF

 

TWINDRIVE® TD4 Advanced USER MANUAL

This User Manual will tell you how to install, use, and maintain your LINAK TWINDRIVE products.

Online Magazine | PDF

 

HOMELINE® accessories

HOMELINE accessories set your bed apart with unique value adding features. Features ensuring comfort and value for the end-user.

Online Magazine | PDF

 

Expanding Your Comfort Zone

Expanding Your Comfort Zone

When it comes to leisure beds LINAK understands the need for safe and reliable actuators systems that work day after day. The TWINDRIVE system is the right system for bed manufacturers.

Online Magazine | PDF

 

TWINDRIVE TD32/TD33 User Manual

TWINDRIVE® TD32/TD33 USER MANUAL

This User Manual will tell you how to install, use, and maintain your LINAK TWINDRIVE® products.

Online Magazine | PDF

Select Your Product:

TD1 Dual Actuator TD3 Dual Actuator

TD4 Advanced

Trouble Shooting TD1


  1. The bed does not work at all
  2. My RF handset does not work
  3. My neck function does not recall correct memory function
  4. How to use the TD1 cable relief
 

The bed does not work at all



Check:
Is the mains connected to the TWINDRIVE TD1?

Try/Solution:
Try to connect a lamp or similar to the mains supply to check that the supply voltage is OK.


Check:
Are all plugs mounted correctly in the TWINDRIVE TD1?

Try/Solution:
Check all connections.


Check:
Are there any visible damages on cables?

Try/Solution:
Damaged parts must be exchanged – contact the company where you bought your bed.

My RF handset does not work



  • The handset needs to be set up to the TWINDRIVE TD1 280 (memory) underneath the bed. Follow the instruction shown in the video or in the text below.


TD1RF 280 (with memory) - How to set up radio frequency handsets


  1. Activate the reset key on the RFR box attached on the TD1
  2. Keep the reset key activated while pressing a random button on the handset
  3. If there are more handsets, keep the reset key activated and press a random button on the other handset. Your bed is now ready for use

- Download above video: TD1RF 280 (with memory) - How to set up radio frequency handsets (28Mb .wmv-file)

Back to top.

 

My neck function does not recall correct memory function



  • The actuator adjusting the neck function needs to be initialized. Follow the instruction shown in the video or in the text below.

TD1RF (with memory) and LA27 – How to initialise the motor system



  1. Drive the LA27 to the outer position (without interruption until it stops)
  2. Release the button
  3. Drive the LA27 to the inner position (without interruption until it stops)
  4. Release the button
The system has now been initialised.

- Download above video: TD1RF (with memory) and LA27 - How to initialise the motor system (42Mb .wmv-file)

Back to top.

TD1 cable relief


By using the cable relief you avoid that the cable plug is pulled out of the TD1 which may lead to a malfunction or damage the plug.

How to use the cable relief – see video.


- Download above video: TD1 cable relief (17Mb .wmv-file)


Back to top.

Trouble Shooting TD3


  1. The bed does not work at all
  2. My handset does not work
  3. The neck function of the bed does not work, it cannot drive outwards
 

The bed does not work at all



Check:
Is the mains connected to the TWINDRIVE TD3?

Try/Solution:
Try to connect a lamp or similar to the mains supply to check that the supply voltage is OK.


Check:
Are all plugs mounted correctly in the TWINDRIVE TD3?
Try/Solution:
Check all connections. Use the cable relief on the TD3 to assure that the cable does not fall out. Follow the instruction shown in the video or in the text below.


TD3 cable relief


By using the cable relief you avoid that the mains cable plug is pulled out of the TD3 and a malfunction occurs.
How to use the cable relief – see video.

Check:
Are there any visible damages on cables?

Try/Solution:
Damaged parts must be exchanged – contact the company where you bought your bed.

- Download above video: TD3 cable relief (14Mb .wmv-file)

Back to top.

My handset does not work


  • The handset needs to be set up to the TWINDRIVE TD3 underneath the bed. Follow the instruction shown in the video or in the text below.

TD3 - How to set up radio frequency handsets


  1. Activate the reset key on the TD3. The bed drives to a flat position. Keep the key pressed until the motor stops completely
  2. Release the reset key
  3. Reactivate the reset key on the TD3
  4. Keep the reset key activated while pressing a random button on the handset
  5. If there are more handsets, keep the reset key activated and press a random button on the other handset

Your bed is now ready for use.

- Download above video: TD3 - How to set up radio frequency handsets (31Mb .wmv-file)

TD3 - How to set up Bluetooth handsets


  1. Plug the Bluetooth Adapter into the powered TD3
  2. The Adapter is now in pairing mode; A blue blinking LED will indicate this
  3. Take the Bluetooth hand control and press the Back Up" and "Down" buttons at the same time. Now the light will give a long blink and indicate that the control and the actuator are paired up

Back to top.

The neck function of the bed does not work, it cannot drive outwards



  • The actuator adjusting the neck function needs to be initialised. Follow the instruction shown in the video or in the text below.

TD3 and LA27 - How to initialise the motor system



  1. Push the down button of the actuator
  2. Drive the actuator until it has reached the inner position and stops completely
  3. Release the key on the handset
  4. Reactivate the down key of the actuator and keep it activated for approx. 5 sec.
  5. You can now drive the actuator outwards
The system has now been initialised.

- Download above video: TD3 and LA27 - How to initialise the motor system (37Mb .wmv-file)

Back to top.

Troubleshooting TD4




TD4 - How to set up a Bluetooth handset:


  1. Set the TD4 in pairing mode by connecting it to the mains
  2. The product is now in pairing mode; The Under Bed Light will blink to indicate this
  3. Take the Bluetooth hand control and press the Back “Up” and “Down” buttons at the same time. Now the light will give a long blink and indicate that the control and the actuator are paired up

Back to top.

For further information please see the HOMELINE User Manuals.
What is a Control
The control is a unit used to control the movements of a LINAK actuator system…
HOMELINE Applications
See examples of HOMELINE applications.
Contact LINAK
Need assistance finding the product that fits your specific requirements?