select
Desk Panel DPT

Desk Panel DPT

The DPT is an innovative DESKLINE® touch panel from LINAK. The panel is the perfect choice for office desks where modern design is the keyword.

The sophisticated solution is based on touch techniques, which are known from e.g. induction stoves and combines high-class design with hich-class techniques, i.e. movement via a simple touch.

The DPT is designed for integration directly in the tabletop ensuring optimal ergonomic use for the end-user. The integration in the tabletop ensures that the panel is completely integrated in the desk design.

The DPT shows the actual desk height in a display. Besides ordinary up-down adjustment, it has 3 memory positions and is compatible with control boxes CBD4, CBD5 and CBD6.

The DPT is available as a 1-channel version for operation of the single or parallel channels. As an end-user service, the 
DPT can show error codes and helps to diagnose possible failures in the system.

desk panel dpt

View the data sheet as an online magazine or download the PDF.

Controls/Handsets USER MANUAL

This User Manual will tell you how to install, use and maintain your LINAK DESKLINE® products.

 

DL1 SYSTEM USER MANUAL

This User Manual will tell you how to install, use and maintain your LINAK DESKLINE® products.

 

DL1A systems user manual

This User Manual will tell you how to install, use and maintain your LINAK DESKLINE® products.

 

DL2 system USER MANUAL

This User Manual will tell you how to install, use and maintain your LINAK DESKLINE® products.

 

 

DL2 and CBD4/CBD5/cbd6 systems
user manual 

This User Manual will tell you how to install, use and maintain your LINAK DESKLINE® products.

 

DL5/DL6 system user manual 

This User Manual will tell you how to install, use and maintain your LINAK DESKLINE® products.

 

DL7 system user manual

This User Manual will tell you how to install, use and maintain your LINAK DESKLINE® products.

 

DL14 system user manual 

This User Manual will tell you how to install, use, and maintain your LINAK DESKLINE® products.

 

DL15/DL16 system user manual

This User Manual will tell you how to install, use and maintain your LINAK DESKLINE® products.

 

DESKPOWER DB4/DL4 systems
user manual

This User Manual will tell you how to install, use, and maintain your LINAK DESKLINE® products.

 

DB5/DB6 system user manual 

This User Manual will tell you how to install, use and maintain your LINAK DESKLINE® products.

 

columns with round profiles system
user manual

This User Manual will tell you how to install, use and maintain your LINAK DESKLINE® products.

 

 

focus on kitchens 

Take your kitchen to the next level.
Only imagination set s limits to how electric movement can improve tomorrow’s kitchen.

 

Trouble Shooting


  1. The desk does not drive at all
  2. The desk can only drive downwards
  3. How to store a memory position
  4. The height in the display is not correct
  5. The display only shows a line (-) and does not work
  6. The desk will not drive the full stroke upwards. Always stops in the same position
  7. The display shows E01 error code instead of the height

The desk does not drive at all


Check: Is the mains connected to the control box?
Try/Solution: Try to connect a lamp or similar to the mains supply to check that the supply voltage is OK.

Check: Are all plugs mounted correctly in the control box and to the leg?
Try/Solution: Check all connections.

Check: Are there any visible damages on cables, controls, the control box or legs?
Try/Solution: Damaged parts must be exchanged – contact the company where you bought your desk.

Back to top.


The desk can only drive downwards



Back to top.


How to store a memory position


  • Favorite positions e.g. for sitting and/or standing can be stored. Follow the procedure shown in the video or in the text below.

How to store a position

How to store:
1. Drive to the height you wish to store
2. Press ‘S’ and then the memory button
Your position has now been stored

To recall your memory position, press the memory button until you reach the stored position.

- Download above video: How to store a position (21Mb .wmv-file)

Back to top.


The height in the display is not correct


  • Correct the height in the display to the actual height of the desk by following the procedure shown in the video or in the text below.

How to set the height of your desk (DP1C and DPT)

Measure the actual height of your desk – from floor to the upper edge of the tabletop
If you have a DPT you need to unlock the control. Follow the procedure shown in the video: How to unlock a DPT desk panel.

1. Press ‘S’ and keep pushing the button until an ‘S’ appear in the display
2. While pushing ‘S’ use the up and down key to change the figure to the actual height

- Download above video: How to set the height of your desk (DP1C and DPT) (14Mb .wmv-file)

Back to top.


The display only shows a line (-) and does not work


  • The DPT is locked when not used to avoid unintented drive. To unlock the DPT follow the procedure shown in the video: How to unlock a DPT desk panel.

Back to top.


The desk will not drive the full stroke upwards. Always stops in the same position



  • The system has set a new end-stop outwards. To erase this position, the desk must be initialised again. Follow the procedure shown in the video: How to initialise your desk.

Back to top.


The display shows E01 error code instead of the height


  • There is a malfunction in the desk. Error code E01 means that the desk must be initialised. Follow the procedure shown in the video: How to initialise your desk.

Should other error codes appear in the display, please consult the user manual for further information.

Back to top.



YouTube video - "How to unlock a DPT desk panel":


How to unlock a DPT desk panel

Unlock DPT
1. Press the ‘S’ button and a figure appears in the display
2. You can now adjust your desk
The desk panel locks itself a few seconds after the adjustment has stopped.

- Download above video: How to unlock a DPT desk panel (7Mb .wmv-file)

Back to top.



YouTube video - "How to initialise your desk":



How to initialise your desk
The desk cannot drive up if it has not been initialised
If display: error code E01

How to initialise:
1. Press down key and drive to the lowest position.
Hold the key until the desk stops completely

2. Reactivate the down key and hold the key until the desk stops completely.
Now the desk can drive up.

- Download above video: How to initialise your desk (16Mb .wmv-file)

Back to top.


For further information please see the DESKLINE User Manuals.
What is a Control
The control is a unit used to control the movements of a LINAK actuator system…
DESKLINE Applications
See examples of DESKLINE applications.
Contact LINAK
Knowledgeable dialogue and close cooperation is the shortest route to a perfect solution.