The DPF1C desk panel is a perfect choice for a wide range of
desks and
workstations with a demand for a panel with height read-out.
The hallmark of the DPF desk panel series is the modern design, which combines classic looks with intuitive, practical use. The up and down buttons have been made extra “user-friendly” as they are shaped “according to the function”, meaning the user can feel the differences and it is not necessary to look when operating the system.
The DPF1C has a display for height read-out in either cm or inches and memory to store the favourite positions.
The display switches off when not in use thereby saving power in standby mode. As an extra feature, the panel can be used for diagnostics as error codes can be displayed.
- The desk does not drive at all
- The desk can only drive downwards
- How to store a memory position
- The height in the display is not correct
- The desk will not drive the full stroke upwards. Always stops in the same position
- The display shows E01 error code instead of the height
Check:
Is the mains connected to the control box?
Try/Solution:
Try to connect a lamp or similar to the mains supply to check that the supply voltage is OK.
Check:
Are all plugs mounted correctly in the control box and to the leg?
Try/Solution:
Check all connections.
Check:
Are there any visible damages on cables, controls, the control box or legs?
Try/Solution:
Damaged parts must be exchanged – contact the company where you bought your desk.
Back to top.
Back to top.
- Favourite positions e.g. for sitting and/or standing can be stored. Follow the procedure shown in the video or in the text below.
How to store a position
How to store:
1. Drive to the height you wish to store
2. Press ‘S’ and then the memory button
Your position has now been stored
To recall your memory position, press the memory button until you reach the stored position.
- Download above video: How to store a position (21Mb .wmv-file)
Back to top.
- Correct the height in the display to the actual height of the desk by following the procedure shown in the video or in the text below.
How to set the height of your desk (DPF1C)
Set the height:
Measure the actual height of your desk – from floor to the upper edge of the tabletop
Set the height:
1. Press the up and down keys at the same time
2. A figure appears in the display
3. Use the up or down key to change the figure to the actual height
- Download above video: How to set the height of your desk - with DPF1C (16Mb .wmv-file)
Back to top.
- The system has set a new end-stop outwards. To erase this position, the desk must be initialised again. Follow the procedure shown in the video: How to initialise your desk.
Back to top.
- There is a malfunction in the desk. Error code E01 means that the desk must be initialised. Follow the procedure shown in the video: How to initialise your desk.
Back to top.
YouTube video - "How to initialise your desk":
How to initialise your desk
The desk cannot drive up if it has not been initialised
If display: error code E01
How to initialise:
1. Press down key and drive to the lowest position.
Hold the key until the desk stops completely
2. Reactivate the down key and hold the key until the desk stops completely.
Now the desk can drive up.
- Download above video: How to initialise your desk (16Mb .wmv-file)
Back to top.
For further information please see the
DESKLINE User Manuals.