PIEZO is a unique hardware based system that will register even the slightest resistance when the desk is driven up or down.
If a PIEZO equipped desk meets an obstacle the system will immediately stop and automatically drive the desk a little bit in the opposite direction. This feature helps you avoid material damage.
Compared to other known systems PIEZO is more sensitive and reacts faster.
The
DL6 No Crossbar,
DL9,
DL11 and
DL16 offer PIEZO as an option. The
column DL14 comes with the built-in PIEZO feature as standard.